AXIS#.WS.IMAX

Description

This parameter defines the maximum current used for wake and shake. If the selected current is too low, the minimum required movement may not occur. If the selected current is too high, the movement may be too fast (overspeed) or too large (over maximum movement).

The maximum of this parameter is the lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK. The default value of this parameter is the half of its maximum. This value depends on the specific application.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Arms

Range

0 to (lower value of AXIS#.MOTOR.IPEAK and AXIS#.IPEAK) Arms

Default Value

(half of maximum) Arms

Data Type

Float
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
AXIS1.WS.IMAX

5013h

0dh

Signed32

-

1000:1

Read/Write

No

AXIS2.WS.IMAX

5113h

0dh

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.WS.IMAX

6703

1A2F

Signed32

Read/Write

-

AXIS2.WS.IMAX

72239

11A2

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.WS.IMAX

6703

Float

Read/Write

-